AXIS#.SAFEPARAM.SLA.FSOE

Description

Indicates if the Safely Limited Acceleration (SLA) safety function can be activated through FSoE. This parameter can only set to “Used” when FSoE is activated (SAFEPARAM.SAFEFIELDBUS.ACTIVATION is set to 1 – “Activated”). When activated, the safety system forbids the axis to move in a negative direction.

Value Description

0

Not used

1

Used

 

Parameters Editor with the FSoE value circled

Context

For complete SLA information refer to SLA (Safely Limited Acceleration).

Related safety parameters:

Versions

Action

Version

Notes

Implemented

2-04-00-000

Implemented in SMM revision v0.56

General Information

Type

Read/Write

Units

N/A

Range

0, 1

Default Value

0 (Not used)

Data Type

Integer

Stored in Non-Volatile Memory

No

Fieldbus Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.SAFEPARAM.SLA.FSOE

3165h

03h

Unsigned8

-

-

Read/Write

No

AXIS2.SAFEPARAM.SLA.FSOE

3265h

03h

Unsigned8

-

-

Read/Write

No